Part # for the DC Jack on the FRDM-K64F

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Part # for the DC Jack on the FRDM-K64F

943件の閲覧回数
vladimirakopyan
Contributor I

Myself and a couple of people on the Mbed site are trying to figure out which part can we use to solder a power jack on J24. A dude asked the question a month ago, but got no answer. Can't find it anywhere in documentation either. Please help.

Mbed Question: Part # for the DC Jack on the FRDM-K64F - Question | mbed

Some more discussion on external pwoer for this board: How to supply the external power to the FRDMK64F board for standalone ? - Question | mbed 

ラベル(2)
3 返答(返信)

673件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Vladimir,

You can download the FRDM-K64F - Printed Circuit Board bill of materials and design files​ and find the Part Number of J24 is PJ1-022.

PJ1-022.jpg

This part number (PJ1-022)  is available in Digikey.

Best Regards,

Robin

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

673件の閲覧回数
vladimirakopyan
Contributor I

Thank you!

0 件の賞賛

673件の閲覧回数
Masmiseim
Senior Contributor I

There is an Excel-Sheet with the BOM of the K64F. Google will help you there.

They use “CON 3 PWR JACK RA TH --- 201H AG 118L” for the Board.

Regards