Hi
Can specific IO can be configured as "DISABLED" if there is no option like this in it's datasheet ?
For example G8:
If not - what is the preffered configuration for savig power (input PD/PU, Output) ?
Another thing - If pin configured as "DISABLED", it is enough for saving power ? or more configurations should be done (PD,PU) ?
Thanks
Edi
Hi
For the G8 pin default function is analog input pin, it could be left floating.
The digital IO pin with default "DISABLE" will saving the power. There does not need to configure related pin, keep default "Disable" setting.
Wish it helps.
Have a great day,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------