本文分享自China-FAE Team,谢谢同事的sharing!
MQX如何自适应10/100Mbps网络
Kinetis K60 媒体接入控制器MAC(Media Access Layer)实现了数据链路层,同时支持10Mbps和100Mbps两种速率。MAC通过MII/RMII接口与PHY芯片连接。
现有的MQX4.0 RTCS协议栈在K60 Tower System Board无法支持与10Mbps交换机等网络设备通信。问题的原因是MQX4.0 BSP初始化代码macnet_init.c默认将MAC配置为100Mbps/Full Duplex模式。
MQX4.0 BSP针对TWR-SER所使用的PHY芯片(KSZ8041NL)的初始化代码没有考虑用户指定链路速率的情况,仅由PHY做默认设置。为了能够自适应链路速率,不仅需要设置KSZ8041NL的控制寄存器(0.13 Speed Select、0.8 Duplex Mode),还要设置K60的ENET_RCR/ENET_TCR寄存器。
解决办法:
修改MQX4.0 BSP代码,使能PHY芯片与网络设备端进行链路速率自动协商,然后读取PHY协议好的链路速率,通过这个链路速率设置MAC的相关寄存器ENET_RCR/ENET_TCR。MQX4.0的 PHY的接口函数已经提供了speed和duplex函数,可供MAC初始化调用,可以保证系统代码的可移植性。
测试结果:
修改后的MQX4.0 BSP代码能够自适应10/100Mbps网络,网络通信正常。
With this code, have you tested the following condition?
1) Boot up K60 with 100/Full Duplex device connected.
2) Disconnect the ethernet
3) Plug in 10/Half duplex device and verify connectivity.