MKW01xxRM reference manual is missing the I2C chapter

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MKW01xxRM reference manual is missing the I2C chapter

597 次查看
theohill
Contributor I

I've got Rev. 2 - 3/2014 which as far as I can tell is the latest edition. There are numerous references to I2C in the manual (for example section 1.9.2), but no chapter describing the operation or memory map.

If it is documented elsewhere or if there is a similar I2C peripheral module that I can substitute the documentation for I'd appreciate being directed to that in addition to this manual being updated.

0 项奖励
回复
1 回复

515 次查看
EarlOrlando
Senior Contributor II

Hello Theo,

You are right, there is a mistake in the MKW01xxRM. I confirm that there are two I2C modules inside the MKW01 MCU, these modules are the same as the included in the KL devices so the information in the MKL26 Reference Manual is valid for this peripheral.

Best regards,

Earl Ramírez.

0 项奖励
回复