Let´s start with KSDK!

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Let´s start with KSDK!

Let´s start with KSDK!

What is it KSDK?

= Kinetis Software Development Kit

Kinetis SDK v2 is a collection of comprehensive software enablement for NXP Kinetis Microcontrollers that includes:

system startup

peripheral drivers

USB and connectivity stacks

Middleware

Real-time operating system (RTOS) kernels.

Documents – Release Note, API Reference Manual, Getting Started with KSDK, for USB – User Guide, USB Composite Device Guide, USB Device Reference Manual and USB Host Reference Manual. All these documents is possible to find at Software Development Kit for Kinetis MCUs|NXP or <ksdk_path>\SDK_2.0_selected_device\docs

KSDK Structure Diagram

pastedImage_4.png

KSDK Features

ARM® and DSP standard libraries, and CMSIS-compliant device header files which provide direct access to the peripheral registers

Open-source peripheral drivers

Open-source RTOS wrapper driver

Real time operation systems (RTOS) including FreeRTOS OS, μC/OS-II, and μC/OS-III

Stacks and middleware in source or object formats including:

CMSIS-DSP -  a suite of common signal processing functions

FatFs - a FatFile System for small embedded systems

mmCAU - Memory-Mapped Cryptographic Acceleration Unit

SDMMC - software component supporting SD Cards and eMMC

DMA Manager - software component used for managing on-chip DMA channel resources

mbedTLS and WolfSSL - cryptographic SSL/TLS libraries

lwIP and USB Stack - a light-weight TCP/IP stack

KSDK Evolution

pastedImage_24.png

KSDK v1/v2 – what new features KSDK 2.0 brings

MQX Kernel removed from KSDK -> focus on FreeRTOS

MQX RTCS Ethernet and MFS File System Stacks -> lwIP and FatFS

OSA, Power Manager and Clock Manager -> no longer required by the drivers

USB Stack re-write -> BSD licensed solution

No platform library -> single project with all needed files

Mbed TLS now included as part of the accelerated cryptography drivers

Eliminates separate HAL and Peripheral Driver -> single driver for each peripheral

Processor Expert -> Kinetis Expert Tool

Updates for KDS -> via online update tool

Installation of KSDK -> KEX Tool (smaller download & sizes)

KEX Tool -> pin muxing selection & generation, clock configuration, low power estimation

pastedImage_65.png

Simplified folder structure

pastedImage_67.png

app.png

KSDK highlights & benefits

Collection of software enablement offered by free

KSDK is fully supported in these IDE:

Atollic® TrueSTUDIO®

GNU toolchain for ARM® Cortex® -M with CMake build system

IAR Embedded Workbench

Keil™ MDK-ARM

Kinetis Design Studio IDE

KSDK supports most of Kinetis MCUs

Created examples for drivers, USB, RTOS, demo applications

Start with development without device register knowledge

Support & download

pastedImage_9.png

Official support of KSDK:

Kinetis Software Development Kit

Create new SR according to:

How to submit a new question for NXP Support

More about KSDK...

KSDK Official Website

www.nxp.com/ksdk

Introducing Kinetis SDK v2

https://community.freescale.com/docs/DOC-329783

Kinetis SDK 2.0 Transition Guide

Kinetis SDK 2.0 Transition Guide

KSDK Community

https://community.freescale.com/community/kinetis/kinetis-software-development-kit

Let´s continue in reading! See Let´s start with FreeMASTER!

标记 (2)
无评分
版本历史
最后更新:
‎04-28-2016 02:44 AM
更新人: