Hello everybody!
I'm working with K60N512, I'm trying to develop an odometer. I guess the best way to accomplish that is with the pulse counter, to measure wheel pulses, and then get the speed and distance with a simple conversion.
But I can not make the counter to increment.
This is how I configure the LPTMR0:
SIM_SCGC5 |= SIM_SCGC5_LPTIMER_MASK; | // Enable LPT Module |
// Reset LPTMR module
LPTMR0_CSR = 0x00;
LPTMR0_PSR = 0x00;
LPTMR0_CMR = 0x00;
// I choose PRESCALER = 1, because it says 0 is not supported on pusle counter mode
LPTMR0_PSR = LPTMR_PSR_PRESCALE(1) | LPTMR_PSR_PBYP_MASK; // bypass glicth filter
LPTMR0_CSR |= LPTMR_CSR_TPS(2); | // Input pin select |
LPTMR0_CSR &= ~LPTMR_CSR_TPP_MASK; // Rising Edge
LPTMR0_CSR |= LPTMR_CSR_TMS_MASK; // Timer as Pulse Counter
LPTMR0_CSR |= LPTMR_CSR_TEN_MASK; // Turn on LPTMR
Then I've got a function generator (square wave) connected to PTC5 (LPTMR0_ALT2), but the counter valur remains zero.
Am I missing something?
Thanks in advance!!
Best Regards,
SebaS
已解决! 转到解答。
Well I figure it out!
The correct value for MUX is 4 and the CMR register must have some value non-zero. So it counts till that value, and sets TCF flag when that value is reached. Also start over counting from zero.
Maybe someone could find it usefull.
SebaS
I've notice I've forgot to enable the PIN, but it is still not working
SIM_SCGC5 |= SIM_SCGC5_PORTC_MASK; //Turn on PORTC clock
PORTC_PCR5=PORT_PCR_MUX(0x3); //Use ALT3 on PTC5
About MUX value, the demo from IAR sets it to be 4... but on K60N512 Reference Manual I can see that it should be 3. What's the rigth value?
Well I figure it out!
The correct value for MUX is 4 and the CMR register must have some value non-zero. So it counts till that value, and sets TCF flag when that value is reached. Also start over counting from zero.
Maybe someone could find it usefull.
SebaS