Kenitis KL05 DMA channel source

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Kenitis KL05 DMA channel source

682 Views
cfk
Contributor I

1.pngHi,i am recently use Kenitis family MCU KL05Z32 , but i conldn't find the dma channel source's details ,neither datasheet nor RM document,where could i find the dma request source of KL05? Could somebody help me?

0 Kudos
Reply
3 Replies

630 Views
migry
Contributor I

Having used DMA in a small number of experimental configurations, and found the documentation "lacking".

I think naming this field as "SOURCE" is confusing.

DMA transfers are triggered by some event, which can include a ALWAYS trigger.

The SOURCE is the source of the TRIGGER.

For some reason the PIT timer gets a special feature in that the TRIG selects the PIT timer overflow as the trigger, but with limitations that you can only use DMA0 with PIT0, DMA1 with PIT1, etc.

While some of the trigger "sources" are obvious, there are a few which I couldn't figure out from the reference manual.

0 Kudos
Reply

606 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

As the section 3.4.8.1 DMA MUX request sources, the source number in Table  20 define the DMA request source.

The DMA triggering source can only be PITx channel, this is a special case, it can manipulate GPIO with PIT cycle.

Hope it can help you

BR

XiangJun Rong

0 Kudos
Reply

651 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

Pls refer to section 3.4.8.1 DMA MUX Request Sources in reference manual of KL05.

Hope it can help you

BR

XiangJun Rong

 

xiangjun_rong_0-1704253019366.png

 

0 Kudos
Reply