KL16 low power crystal startup time

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

KL16 low power crystal startup time

612件の閲覧回数
chipweller
Contributor II

I am using a MKL16Z256VLH4 with a 32768 Hz crystal running in lower power mode (HGO=0).  The datasheet lists the typical crystal startup time (tsct) as 750 ms, and I do see something like that.

My question is what should I assume for the maximum time. Currently I am using 1 second. The processor is running at 3.0V (+/-4%) and the expected die temperature range is 15C to 45C.

Thanks

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

463件の閲覧回数
Paul_Tian
NXP Employee
NXP Employee

Hi, Weller

Sorry, we do not provide max. value of startup time. But I think you can use this 1 second value first. Thanks.

Best Regards

Paul

0 件の賞賛
返信