Need Sample Code to transmit and Receive CAN messages using KEA128 Micro Controller. IDE used is KEIL.
Hi kerryzhou,
I am doing various development tests with the TRK-KEA128 board.I have a few questions.
Can you help?
Hi Sharad Mehta,
We still don't have the keil MSCAN project for KEA128, but we have a lot of CAN drivers, and some other IDE project, take an example CW MSCAN project.
You can find the KEA128 MSCAN driver from this link::
MSCAN driver for Kinetis EA devices
The above link already contains the CW KEA128 MSCAN project, you can test it on our TRK-KEA128 board.
But if you still want to use the keil project, I think you can create a keil project, then add the above CAN driver to your keil project, then test it.
Beside the above MSCAN driver, in the attachment, I also attach another CAN CW project, it also has the CAN driver, just different format, it also works.
Wish it helps you!
Have a great day,
Kerry
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi , I want to use the sample code "Can_test_nonemask250k.rar" , What version of CodeWarrior should I download, thanks.
CW for MCU 10.5
Hi kerryzhou,
I am doing various development tests with the TRK-KEA128 board.I have a few questions.
Can you help?
What code do I need to add to CAN_Node1_demo.c to use Systick?
Have a great day