Hi,
I am using a K20 based MK20FN1M0VMD12
I am using the flexbus to connect to an SRAM chip. I am using the following pins for control signals to the SRAM
Pin name | ALT Mode | Function |
PTD1 | ALT 5 | FB_CS0_B |
PTC11 | ALT 5 | FB_RW_B |
PTB19 | ALT 5 | FB_OE_B |
PTC17 | ALT 5 | FB_BE31_24_B |
PTC16 | ALT 5 | FB_BE23_16_B |
I am using these pins in the ALT 5 mode, I need to have high drive strength on these control signals.
I found in the datasheet that bit 5 of the pin control registers need to be set to 1 for high drive strength.
PORTx_PCRy[n] x = port letter y = pin number n = register bit# |
My question is, although I am operating in ALT 5 mode for these pins, can I still enable high drive strength on these pins by setting the corresponding (bit 6) PCR bits? i.e.
FB_CS0_B | PORTD_PCR1[6] = 1 |
FB_RW_B | PORTC_PCR11[6] = 1 |
FB_OE_B | PORTB_PCR19[6] = 1 |
FB_BE31_24_B | PORTC_PCR17[6] = 1 |
FB_BE23_16_B | PORTC_PCR16[6] = 1 |
Will these pins have high drive strength if I set bit 6 of these registers to high(1)? (I am using ALT5 function of these pins for flexbus SRAM control signals)
Thank you for your time.
解決済! 解決策の投稿を見る。
Hi Sherry,
It's ok to set the bit 6 to 1 when pin work in the ALT5 mode.
The Driver Strength Enable (DSE) is valid in all digital pin muxing modes, definitely contains the ALT5.
Hope it helps.
Have a great day,
Ping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Sherry,
It's ok to set the bit 6 to 1 when pin work in the ALT5 mode.
The Driver Strength Enable (DSE) is valid in all digital pin muxing modes, definitely contains the ALT5.
Hope it helps.
Have a great day,
Ping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks Jeremyzhou,
That answers my question perfectly.