Hi,
I just purchased a Freedom KL25Z dev unit (FRDM-KL25Z) and am trying to use it. I am following NXP's provided Getting Started Guide located here
Getting Started Guide
FRDM-KL25Z|Freedom Development Platform|Kinetis MCU|NXP
Current State (Stuck!)
I have installed the IDE and Toolchain and have gotten to try to build my own project. I can build the lib (ksdk_platform_lib_KL25Z4), but the Linker fails on all attempts (hello_world attempt)!
See attached 'getting started procedure - trial 1.txt' for fairly detailed notes on my procedure leading up to failure. I've re-tried this a second time, and it failed again.
Request
Help, please!! What am I doing wrong, and how to correct?
This is like "Hello World 101", and is embarassing that I am stuck. Any and all help is Greatly appreciated!!
-Justin
Original Attachment has been moved to: getting-started-procedure---trial-1.txt.zip
已解决! 转到解答。
Hi Justin,
have a read at https://mcuoneclipse.com/2016/08/01/bricking_and_recovering_opensda_boards_in_windows_8_and_10/ , I think this should solve your problem (I hope), at least I was able to recover on my side.
I have added a short video with the steps to the above post too.
I hope this helps,
Erich
Hi Justin,
Great to hear that it works now, and I hope you enjoyed your beer.
I'm sorry, I did not know that the group policy editor is only part of the Pro Edition :-(. Googling around I see that Microsoft does that already from Windows Vista on that way. And I feel very sorry that you had to spend money for an Windows update. I hate to write that after some googling that was not really necessary, as it is possible to make that change in the registry (regedit) as well. I hope that in the home edition using regedit is possible too? I have updated the the post with a section "Using Windows Registry" so this way is documented too.
Erich
this may sound cheesy but it's serious, as long as the final delivered solution, your article, provides the solution, it is totally fine by me! The money invested by me here is simply an investment in my machine and workstation, in review :)!
Hi Justin,
if you are using Windows 10, then this explains everything. That problem started with Windows 8 (see https://mcuoneclipse.com/2013/10/12/frdm-board-bootloader-fails-with-windows-8-1-preview/ ). I still have a notebook with Windows 7 around for this kind of problems (NXP is not the only company facing this problem: lots of hardware/boards produced before Windows 8 have this kind of problems).
There is one thing you could try (noted in comments of https://mcuoneclipse.com/2014/11/01/illustrated-step-by-step-instructions-updating-the-freescale-fre... ):
check out http://answers.microsoft.com/en-us/windows/forum/windows8_1-hardware/how-do-i-prevent-system-volume-... if this works on your machine (I have not tried that myself).
I hope this helps,
Erich
Hi Justin,
stay tuned! I think I have found a way how you can recover the board without the need for a Windows 7 machine. I'm drafting right now an article and hopefully I can publish it on http://mcuoneclipse.com/ tonight (we have a national holiday today).
Erich
Hey Erich,
Are we serious here? THIS IS RAD, THANK YOU!!! I'll be around if needed to test, inspect or give feedback on anything! Just contact my by email if needed for faster response :smileyhappy:
-Justin
Hi Justin,
yes, I have ordered a new board from Farnell to see what happens, it arrived today.
My FRDM-KL25Z board had the V1.09 bootloader (the old one). This happened to me (please if this is the same for you):
a) originally plugin in the board, the small green LED came up, and board was recognized properly
b) powering it up in BOOTLOADER mode (Reset pressed), the board came up as BOOTLOADER, then the green small LED is off for a while, then blinks an error code, then off again, etc
c) in BOOTLOADER mode, clicking on the info.html file, it shows a version of 0.00 for the application in the web browser
d) powering the board normally, it does not enumerate, and the small green LED is always off (board bricked)
Same for you?
Erich
In short, yep. In more detail -
I plugged in OpenSDA-USB to a powered down board, let Windows recognize the board and then inspected in File Explorer and Device Manager. Both boards displayed the same result for the two configurations of RST
RST depressed:
RST not depressed:
No response, they both appear bricked. No enumeration, no LEDs, nadda!
What may be the root cause here, sheesh! :smileysad:
Hi Justin,
have a read at https://mcuoneclipse.com/2016/08/01/bricking_and_recovering_opensda_boards_in_windows_8_and_10/ , I think this should solve your problem (I hope), at least I was able to recover on my side.
I have added a short video with the steps to the above post too.
I hope this helps,
Erich
Yikes!! ... this is immensely embarrassing, and perceivably naive - how do you access the Group Policy Editor (gpedit) in Windows 10?? I have spent almost ten minutes now trying to uncover it and every google search result of a how-to fails... XX(! #1 how on earth can they all fail, and #2 why am I so bad at this?
Erich, if you could help, I would immensly appreciate it. As I can't open gpedit, I can't try your solution!! :smileysad:
EDIT (update & gpedit soln): Well after 10 minutes with MS tech support, it appears that the Group Policy Editor is a feature restricted to Windows 10 Pro, sheesh! So if you have the Home edition as I did, you will need to for over $99.99, yikes. I did, now I'll give Erich's solution here a try!! :smileyhappy:
Hi Dan,
I tried your FW update procedure outlined by MCUonEclipse on this board this morning, but dang it, this didn't work.
Here was the result
ok, must be a bad board right? Welp, nope... my second board came from Digikey this morning. I repeated the same process with this board, AND IT FAILED FOR THIS BOARD TOO! See 'newBoard_steps.txt' for detailed procedure for connecting and trying the new Digikey board this morning.
One interesting note
Questions / Next Steps
One question of curiosity
Woe is me, please help me get up and running!! This is embarassing, and it is sad... XX(!!
Hi Justin,
maybe I have missed it, but what host operating system are you using?
You only need to update the FRDM-KL25Z board bootloader if you are using Windows 10 or 8, but you need a Windows 7 machine for the update of the bootloader!
So can you confirm you are using a Windows 7 machine?
Here a few things where we could identify the problem:
1) Power/Plug in the board with the reset button pressed. It shall show up as BOOTLADER, with the following device in the device manager:
2) If you power the board with the P&E firmware loaded, it shall show up as FRDM-KL25Z, with the following devices:
For the copy operation outlined in https://mcuoneclipse.com/2014/11/01/illustrated-step-by-step-instructions-updating-the-freescale-fre..., do not use the file from the zip file directly. Unpack the files first. Use the DOS cmd.exe copy command and not the Windows Explorer. Disable any explorer extensions, firewalls or virus scanners.
In the debug connection, you have to use OpenSDA as interface:
I hope this helps,
Erich
Hi Dan,
In prep for the arrival of my new FRDM-KL25Z and FRDM-KL82Z tomorrow, I wanted to take the safest possible path forward, to ensure I don't fail again with these boards ;)!
I've written up my detailed and explicit, perhaps semi-verbose procedure for tomorrow, I've attached it (getting started procedure - rd 3.txt), could you take a peek and let me know your thoughts? My expectation is that this is super-over-the-board on detail, just plug, play then run, but I cannot fathom the terror and fear that may come from a second failure! Sheesh!! ;)!
Could you review the attached proposed procedure for tomorrow, and let me know if ok? :smileyhappy:
Thanks,
Justin
Hi Justin:
The factory boards come shipped with an outdated firmware and application, To make the board working with Windows 8 it requires a bootloader update. To really use the board, the latest firmware needs to be loaded on the board too. could you try to update the firmware to see whether it helps?
Here is the step by step guide by my colleague.
Regards
Daniel
Hey Dan,
I reinstalled the drivers following your instructions, validated the drive in File Explorer and the two items in Device Manager.
Present Items after driver reinstall
Still no ports showing up for my debug launch, same as last time. Yikes, thoughts?
To note your LED is on in your picture, mine stays off. Also to note, I have purchased a new FRDM-KL25Z board, should be in within a few days.
Sheesh / thank you!! :smileyhappy:
OpenSDA supports two modes
These two are called OpenSDA applications.
To use the debugger application you need to load it into the OpenSDA chip.
For that press and hold reset button and connect usb cable to OpenSDA USB. This will also install as USB drive, but this time it won't program the target MCU but program the OpenSDA MCU.
From the following link you can download latest OpenSDA applications
http://www.pemicro.com/downloads/download_file.cfm?download_id=378
Find the correct application file for your Freedom Board (MSD-DEBUG-FRDM-KL25Z_Pemicro_v118.sda)
and copy/paste to the BOOTLOADER flash drive
WAIT TILL FULL FILE IS TRANSFERRED!Then disconnect and reconnect. Now it will work like a debugger and not a flash programmer.