How will Qualcomm's possible acquisition of NXP affect all of us?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How will Qualcomm's possible acquisition of NXP affect all of us?

1,006件の閲覧回数
dave408
Senior Contributor II

I started my ARM experience with the Freescale Kinetis line, which was purchased by NXP, and thankfully, things have continued smoothly from my perspective.

Now that Qualcomm is likely going to acquire NXP, do I need to worry about how this will affect projects like KDS, as well as the Kinetis line of processors?

Qualcomm to Acquire NXP | Qualcomm 

ラベル(2)
0 件の賞賛
返信
4 返答(返信)

534件の閲覧回数
soledad
NXP Employee
NXP Employee

Hello Dave,

Regarding the changes to the company's products, from the perspective of our customers, we believe that this combination will enable us to become an even stronger partner for you, enabling us to broaden and deepen our leading product platforms, while strengthening and expanding our distribution channels. As there is little product overlap between the two companies, and several products and technologies are complementary, we expect to provide our customers with an expanded set of solutions.

We expect to honor all existing NXP longevity commitments on product supply to meet the requirements of the Automotive, Medical, Telecommunications and Industrial markets that will be extremely important markets for the combined company.


Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

534件の閲覧回数
michaelheidinge
Contributor III

@soledad

Actually since Qualcom is taking over NXP, and now Broadcom, I'm afraid the products won't be updated further. No real "bummer" came out, however there are so many things that could be improved.

-Real low cost MCUs with DMA and real low power

-Lower power consumption M4

Actually for me now, Microchip seem to come out with really nice ARMs. When will you also offer an M4 with <70µA/MHz? Current consumption is round 400µA/MHz for mine.

NXP, if don't keep updating the MCUs, users will switch to other vendors. Currently I would choose another brand for a the next product development, as performance is (µA/MHz) and value is better.

0 件の賞賛
返信

534件の閲覧回数
jamesbone
NXP TechSupport
NXP TechSupport

Hello Michael,

NXP has another ARM  family processor,  in this case it is the LPC  Family   LPC5411x MCU can shut down the Cortex®M4 for a tiered power approach and use the Cortex®  -M0+ to perform less taxing tasks, achieving an even lower active mode of 60 μA/MHz.

Here is a link to the web page of the LPC 54xx family.

LPC54000|Low Power 32-bit MCUs|Cortex-M4 Core|NXP 


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

534件の閲覧回数
mjbcswitzerland
Specialist V


Haven't heard much about the Qualcomm takeover stuff in the meantime but it looks like Broadcom is now trying to take over Qualcomm:
https://www.bloomberg.com/news/articles/2017-11-06/broadcom-offers-130-billion-for-qualcomm-in-landm...

Regards

Mark

0 件の賞賛
返信