Hello,
I have a KV56 project and I'm trying to get the clock tool running with it to generate the clock_config files but when I click on MCUXpresso Config Tools I get this message:
I took the clock_config files from the sdk examples and modified my oscillator frequency to me external oscillator of 12MHz.
This does allow the debug console to work, but I'm afraid I missed something. I also set board XTAL_FREQ to 12MHz
However, when I check CLOCK_GetCoreSysClkFreq it is not close to 240MHz for the HS clock.
Solved! Go to Solution.
I figured out that I could go online and do this in the SDK builder there's an option to "explore KV56" and then generate the code
Nope! I figured it out!
I figured out that I could go online and do this in the SDK builder there's an option to "explore KV56" and then generate the code
I see you already figured it out, do you have another question about it?