Hi,
Please check attached KL series COP validation code.
And you could find KL26 ADC example code at KL26 sample software [FRDM_KL26Zdemo] project, major at <adc_test.c>. (KL15 using the same ADC module with KL26)
The KL26 sample code could be downloaded here.
Have a great day,
best regards,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
#include <inttypes.h> to get the format specifiers for your compiler.
Explained here: Formatted output when using C99 data types « Stack Overflow
Hi,
i were checking the <adc_test.c> example but it doesn't seem right.
uint16 adc_read(uint8 channel)
{
ADC0_SC1A = !AIEN_ON | DIFF_SINGLE | ADC_SC1_ADCH(channel) ; // start conversion
while((ADC0_SC1A & ADC_SC1_COCO_MASK)!= 0){};
return ADC0_RA;
}
Page 453 of KL15P80M48SFORM.pdf
7 COCO
Conversion Complete Flag
Field Description
This is a read-only field that is set each time a conversion is completed when the compare function is
disabled, or SC2[ACFE]=0 and the hardware average function is disabled, or SC3[AVGE]=0. When the
compare function is enabled, or SC2[ACFE]=1, COCO is set upon completion of a conversion only if the
compare result is true. When the hardware average function is enabled, or SC3[AVGE]=1, COCO is set
upon completion of the selected number of conversions (determined by AVGS). COCO in SC1A is also set
at the completion of a calibration sequence. COCO is cleared when the respective SC1n register is written
or when the respective Rn register is read.
0 Conversion is not completed.
1 Conversion is completed.
So we start conversion and wait while Conversion is completed...
Hi,
For the ADC module operation, customer could enable ADC interrupt mode.
When ADC module finish the conversion and will generate an interrupt, in interrupt service routine, the ADC conversion result could be read out.
The FRDM_KL26Z board ADC demo is using the interrupt mode, customer could download related code here.
Wish it helps.
Have a great day,
best regards,
Ma Hui
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
hi,
I tested ADC code in FRDM_KL25Z board and seems to be working well, but not so good in my custom board with MKL15. The values are always in overflow state (0xFFFF) and i don't understand why.
I tried to read TempSensor, ADC0_SE8/PTB0 and ADC0_SE13/PTB3 inputs using Generated Code by Processor Expert.
Thanks for your attention.
Best Regards,
Rui Faria