FreeRTOS-LWIP fails to receive big data

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FreeRTOS-LWIP fails to receive big data

Jump to solution
1,986 Views
jake111
Contributor I

I'm using MK64FN1M0VMD12,and read data from server by LWIP running on FreeRTOS.

LWIP version:2.2.0

FreeRTOS kernel version:10.2.0

The server sends data to client by TCP every one second.When the data transfers at the rate of about 100bps,it works well for a long time.

But a timeout occurs when the speed is larger than 200bps.At this moment,lwip_read will always timeout,and reconnecting TCP will always fail until you reboot the system.

Sometimes it can only receive 2000 bytes then a timeout occurs,but sometimes it can receive more than 100000 bytes then a timeout occurs.

the code is roughly like this:

socket = socket(AF_INET, SOCK_STREAM, 0);
connect(socket, (struct sockaddr *)&addr, sizeof(struct sockaddr));
setsockopt(socket, SOL_SOCKET, SO_RCVTIMEO, &tv, sizeof(tv));

/* write to the server to request sending messages to client every second */
write(socket, buf, len);
/*  */
while(1)
{
	read(socket, buf, BUF_SIZE);
}

What is the most likely cause of the problem?

0 Kudos
Reply
1 Solution
1,932 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @jake111,

There could be a lot of causes for this timeout issue. Are you using a custom board or the evk for the MK64? Is this implementation yours, or are you utilizing an example? If it is, could you please try an example from the SDK and tell me if the problem is still present?

The lwip_enet_iperf3 example provides basic commands to measure performance of network stack. With this example, you can get an idea of how much throughput your device provides with your characteristics. Could you please test this and tell me how much throughput you get?

The timeout error could be caused by the physical connection of your circuits being damaged, so please take that into consideration aswell.

I hope you find this helpful!

Best regards, Julian

View solution in original post

0 Kudos
Reply
1 Reply
1,933 Views
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @jake111,

There could be a lot of causes for this timeout issue. Are you using a custom board or the evk for the MK64? Is this implementation yours, or are you utilizing an example? If it is, could you please try an example from the SDK and tell me if the problem is still present?

The lwip_enet_iperf3 example provides basic commands to measure performance of network stack. With this example, you can get an idea of how much throughput your device provides with your characteristics. Could you please test this and tell me how much throughput you get?

The timeout error could be caused by the physical connection of your circuits being damaged, so please take that into consideration aswell.

I hope you find this helpful!

Best regards, Julian

0 Kudos
Reply