Customer asks about Kinetis L series with 16 bit ADC: A lot of the literature I see is about the impedance presented to the front end of the (capacitive SAR) ADC. But I think what really happens is a charge transfer from the source storage cap to the ADC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Customer asks about Kinetis L series with 16 bit ADC: A lot of the literature I see is about the impedance presented to the front end of the (capacitive SAR) ADC. But I think what really happens is a charge transfer from the source storage cap to the ADC

2,267 Views
steve_fae
Senior Contributor I

Customer writes:

Regarding 16 bit ADC, charge distribution. A lot of the literature I see is about the impedance presented to the front end of the (capacitive SAR) ADC. But I think what really happens is a charge transfer from the source storage cap to the ADC input sampling cap. It's always modeled as Z but to me this is a time-domain problem, and one I no longer understand.

 

All of our sources (things we want the ADC to measure) have a 0.1uF cap. That's several orders of magnitude greater than the ADC sampling cap. It would seem to me that, regardless of the source impedance (several k), there is sufficient coulomb storage.  Is there an APP that addresses or discusses this further?

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,919 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Steven,

I think the an4373.pdf is helpful to understand the charging between external capicitor and capicitor of S/H.

Hope it can help you.

BR

XiangJun Rong

0 Kudos
Reply