I have a project that was built with a Segger Jlink for hardware connection. I only have access to OSBDM or a PEMicro universal multilink. Is there a script to follow in order to modify the project settings to change the build to use what I have access to?
I am stuck at this stage. I don't know how to import something from lets say a project that is already configured correctly.
已解决! 转到解答。
Hi,
The connection configuration looks ok. Do you have the two Multilik led's on?
I think you can do two things:
1) Create a new project with CW wizard and try to connect.
2) Enable log in debug connection to see what error is reported
How are you powering the TWR?
Luis
Hi,
You can create a new connection like in your screen attached, completing the target device and the hardware debugger interface or just change the hw in the segger existing connection. Go to debug configurations > Select the configuration for Segger > press Edit button and in the Connection Type, select P&E instead of Jlink.
That's all.
Best Regards,
Luis
so I changed the settings from jlink to PE multilink but it won't connect
first captures shows setting second shows connection error
what i have in hand is a universal multilink but it seems to have found an FX??
Hi,
The connection configuration looks ok. Do you have the two Multilik led's on?
I think you can do two things:
1) Create a new project with CW wizard and try to connect.
2) Enable log in debug connection to see what error is reported
How are you powering the TWR?
Luis