"Hello World" built on KDS Environment

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

"Hello World" built on KDS Environment

2,452 Views
kenhsu
Contributor II

I import the project from C:\Freescale\KSDK_1.3.0\examples\frdmkl03z\demo_apps\hello_world

and built "Hello World" on my KDS enviroment. Get following result, but import KL03 lib and built are OK. Where to check makefile?

 

11:29:53 **** Incremental Build of configuration Default for project hello_world_frdmkl03z ****

make all

Cannot run program "make": Launching failed

 

 

Error: Program "make" not found in PATH

PATH=[C:/Freescale/KDS_3.0.0/eclipse//features/com.somniumtech.jre.win32.win32.x86_1.7.0.76/jre/bin/client;C:/Freescale/KDS_3.0.0/eclipse//features/com.somniumtech.jre.win32.win32.x86_1.7.0.76/jre/bin;C:/Freescale/KDS_3.0.0/eclipse//features/com.somniumtech.jre.win32.win32.x86_1.7.0.76/jre/lib/i386;C:\Program Files (x86)\Intel\iCLS Client\;C:\Program Files\Intel\iCLS Client\;C:\Windows\system32;C:\Windows;C:\Windows\System32\Wbem;C:\Windows\System32\WindowsPowerShell\v1.0\;C:\Program Files (x86)\Intel\OpenCL SDK\2.0\bin\x86;C:\Program Files (x86)\Intel\OpenCL SDK\2.0\bin\x64;C:\Program Files\Intel\Intel(R) Management Engine Components\DAL;C:\Program Files\Intel\Intel(R) Management Engine Components\IPT;C:\Program Files (x86)\Intel\Intel(R) Management Engine Components\DAL;C:\Program Files (x86)\Intel\Intel(R) Management Engine Components\IPT;c:\Program Files (x86)\Microsoft SQL Server\100\Tools\Binn\;c:\Program Files\Microsoft SQL Server\100\Tools\Binn\;c:\Program Files\Microsoft SQL Server\100\DTS\Binn\;C:\Program Files (x86)\UltraEdit;C:\Program Files (x86)\Windows Kits\8.1\Windows Performance Toolkit\;C:\Program Files\Microsoft SQL Server\110\Tools\Binn\;C:\Program Files (x86)\Microsoft SDKs\TypeScript\1.0\;C:\Freescale\KDS_3.0.0\eclipse;]

 

 

11:29:53 Build Finished (took 78ms)

 

Sincerely

Ken

Labels (1)
0 Kudos
Reply
15 Replies

2,031 Views
kenhsu
Contributor II

Hello Alice,

        No, no..., our board is not a demo board, we designed following the vendor circuit. and currently can run MultiLink Universal.

Sincerely

Ken

pastedImage_0.png

0 Kudos
Reply

2,031 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

HI Ken,

Ok, if the simple project you creates work well on your board , while the KSDK1.3 demo

can not work , it is much possible the KSDK problem , please re-install it , and please

also take a screenshot or video  show us how do you download and install .

BR

Alice

0 Kudos
Reply

2,031 Views
kenhsu
Contributor II

Hello Alice,

     Currently I used the demo under KSDK1.3.0, not KSDK1.2.0. I didn't have OPENSDA on my site, I always used MultiLink.

Sincerely

Ken

0 Kudos
Reply

2,031 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi Ken,

KSDK1.3 is OK, the FRDM-KL03 board have OpenSDA , you need nothing else.

You only need connect the board and your PC like this :

pastedImage_0.jpg

then check the Device Manager of your PC:

pastedImage_2.png

Please also check the place Michal Zan mentioned .

BR

Alice

0 Kudos
Reply

2,031 Views
michalzan
NXP Employee
NXP Employee

Hi Ken,

please look into Window->Preferences->C/C++->Build->Global Tools Path. Are there following paths?

Capture.PNG

Michal

0 Kudos
Reply

2,031 Views
kenhsu
Contributor II

Hello Alice,

     Here is my Debug Configuration

pastedImage_0.png

Sincerely

Ken

0 Kudos
Reply

2,031 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

Let's reconstruct the problem.

When you create one new simple project , it can work well when build and debug , you must be

sure whether it can work well when debug .

While when import the demo under KSDK1.2 installation directory , it have error , am i right ?

If yes, maybe the KSDK have some problem when installation , i recommend you install the KSDK1.3 or Ksdk2.0.

If the new simple project also can not download and debug well , please try use the OPENSDA on your board to

debug , only need connect the board and PC USE one USB cable. (use this method test the simple project and the KSDK demo ).

Alice

0 Kudos
Reply

2,031 Views
kenhsu
Contributor II

Hello Alice,

     I don't know where I already modified on KDS Environment. you mention screenshot can show up and I need to add some include path in, but still cannot be built(even delete project, then import again, still have the same issue).

      Then I try to Import another project of hwtimer_demo, which built is OK, and I meet a problem.

PE-ERROR: Error downloading to the device.

pastedImage_0.png

Sincerely

Ken

0 Kudos
Reply

2,031 Views
MarekTrmac
NXP Employee
NXP Employee

Hi Ken,

does you KSDK support KDS? Have you downloaded KSDK from KEx builder web site? Have you selected KDS as toolchain?

Regards,

Marek

0 Kudos
Reply

2,031 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Ken,

Which debug mode do you used ? Please take a screenshot about the debugger configuration :

pastedImage_0.png

BR

Alice

0 Kudos
Reply

2,031 Views
kenhsu
Contributor II

Hello Alice,

     I used Win7. If I create a simple project, which built is OK.

If Import APP code from KSDK 1.3.0, which project cannot show above page, but a simple project is OK.

pastedImage_0.png

Sincerely

Ken

0 Kudos
Reply

2,031 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Ken,

Are you sure have install the ksdk in to the KDS , the detail steps you can refer to this DOC(KDS_3.0.0\doc)

"KDS_Users_Guide.pdf" ->4.2 Installing Kinetis SDK into KDS

If still have problem, recommend you install the latest version of KDS3.2.0 :

New Kinetis Design Studio v3.2.0 available

Hope it helps

Alice

0 Kudos
Reply

2,031 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Ken,

Does the KL03 lib is KSDK1.3 lib ?

If not , please first build the KSDK1.3 lib , it under the KSDK1.3:

Freescale\KSDK_1.3.0\lib\ksdk_platform_lib\kds\KL03Z4

If you build this lib , it still have problem , please check and show the "Console" view,

also take a screenshot tell me the steps you do .

Hope it helps

Alice

0 Kudos
Reply

2,031 Views
kenhsu
Contributor II

Dear Alice,

     Yes, I built lib is KSDK1.3 lib and path is C:\Freescale\KSDK_1.3.0\lib\ksdk_platform_lib\kds\KL03Z4.

Screenshot is as below.

Sincerely

Ken

pastedImage_0.png

0 Kudos
Reply

2,031 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Ken,

What about your PC system?

And could you create one simple bare board project(without KSDK) ,

check whether it can work well ?

Also what about create one KSDK project by yourself ?

Please check there :

pastedImage_0.png

If all of the project have error when build , i recommend you re-install the KDS and KSDK .

Hope it helps

ALice

0 Kudos
Reply