programming connections for MKE04 series

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

programming connections for MKE04 series

1,586 Views
jamespottebaum
Contributor I

how to you provide for programming of the MKE04 series of micros

can not find any documentation anywhere - - -

 

what combination of pins needs to be brought out.

 

also what interface module is needed to program the PCB from a PC

 

Jim P

Labels (1)
0 Kudos
Reply
5 Replies

966 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi James,

we can use Multilink Universal or  Multilink Universial FX to program KE04

P&E Microcomputer Systems - USB Multilink Universal - USB Multilink Universal All-In-One Development...

P&E Microcomputer Systems - USB Multilink Universal FX - USB Multilink Universal FX All-In-One Devel...

we can refer FRDM-KE04Z schematic SWD design for how to design program interface.

http://cache.freescale.com/files/soft_dev_tools/hardware_tools/schematics/FRDM-KE04Z_SCH.pdf

if you already purchased FRDM-KE04Z board, you can debug and program KE04z via OPENSDA usb interface, needn't external programmer.

Freescale Freedom Development Platform for th|Freescale

can this help?


Have a great day,
Zhang Jun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

966 Views
jamespottebaum
Contributor I

that helps.

looking at the FRDM-KE04Z, do I have to add the 10 pin micro connector?

Jim P

0 Kudos
Reply

966 Views
DavidS
NXP Employee
NXP Employee

Hi James,

The FRDM-KE04Z Freedom boards have on-board debugger capability via the USB connector.  You do not need to populate the 10-pin header.  The USB provides power, debugging, Virtual COM Port, and debugger firmware update capabilities.

For a custom product you develop, then you would need to have a 10-pin debugger header that will work with PEMicro, Segger, and other debugger hardware.

Regards,

David

0 Kudos
Reply

966 Views
jamespottebaum
Contributor I

I am developing my own board and need to program it - - - -

from the pictures, the 10 pin programming connector is not installed on

the FRDM - - - -

can I install it and use it to program my own MKE04 design

Jim P

0 Kudos
Reply

966 Views
DavidS
NXP Employee
NXP Employee

Seems like it would work.

Please review this great blog (and signup for it too).

Using the Freedom Board as SWD Programmer | MCU on Eclipse

Regards,

David

0 Kudos
Reply