Dear Sir,
I can debug,RUN and FLASH using code warrior development studio.But i can only use debug mode in kinetic development studio.
in project properties of KDS configuration in C/C++ build is Debug is active .there is any other option there.In codewarrior configuration c build is RAM,FLASH,debugg is there. I have doubt that in KDS no tool or settings to flash and run the code.i am using K40(kinetic kwikstik)
please tell me how to solve the problem
For what it's worth, I tend to use "Debug" anyway. However, on my K22F board, I have difficulty getting it to run without actually being in the debugger. When I download flash, or disconnect, the board never runs. I have to manually press reset. While I can work with this, at least for now, it is not behavior I am accustomed to. With any Atmel development I have done, when I download code or stop debugging, the processor always resets and begins normal execution of code.
Perhaps I am missing something? I guess I could try Erich's trick and create a debug config and make it work that way.
Hi Tharon,
Other IDE's for Kinetis have that capability to run after disconnecting but from my experience KDS does not yet.
Hopefully in future.
Regards,
David
Hi Sir,
That means KDS has no facility to load the code into flash and it not gives facility to RUN and KDS giving only debugging facility.Is it right ? Please tell me.Its urgent because i actually working to program k40 controller.Thank you
With KDS you can load the code into FLASH, and you can run it, and you can debug it.
Dear sir,
Then what is the reason it does not load flash and I can only able to debug code.There is no break points.It actually by means RUN the code .I think the code working in RAM area .Then I try to flash the .elf file generated using KDS by codewarrior .It successfully load the code into flash but not working. But .elf file generated using codewarrior able to flash and its working
Hi again Lijo:
Are you still having problems loading code to KwikStik K40?
If so, please share your project with us. In any case I would like to recommend you the latest version of KDS (KDS v3.0.0):
Kinetis Design Studio Integrated Development |Freescale
Or you could still use CodeWarrior for MCU:
CodeWarrior for Microcontrollers-Eclipse IDE|Freescale
Regards!
Jorge Gonzalez
hello,
I tried this settings not working in kinetic design studio.I changed to different settings change but not working