Hi,
As question above, what is internal flash ram range on mk20dx256vll10. I didnt find on datasheet.
I've been trying all addresses on memory map, but Processor expert just doesnt like it. By the way,
I am trying to figure out a way to make an usb bootloader on KDS with processor expert.
Thanks,
Yaran
Hi Yaran,
Please look at the chip/device Reference Manual:
http://cache.freescale.com/files/32bit/doc/data_sheet/K20P100M100SF2V2.pdf
Chapter 3.5.1.2 Flash Memory Sizes
FlexRAM address range is 0x1400_0000 - 0x1400_0FFF.
It can be used as generic RAM when not used as part of the FlexNVM functionality (aka EEPROM window).
Regards,
David