Dear All,
I am trying to import a CW project into KDE 3.0 and getting following@ error.
Description Resource Path Location Type
make: *** No rule to make target `MyWirelessApp Demo Coordinator - Security Enabled.elf', needed by `main-build'. Stop. MyWirelessApp Demo Coordinator - Security Enabled C/C++ Problem
Any help would be highly appreciated.
Thanks,
Salah
Using a CodeWarrior project in KDS v3.0.0 will need that you convert that project, see the CodeWarrior converter manual.
See C:\Freescale\KDS_3.0.0\doc\KDS_Porting_Guide.pdf
As for the 'no rule' message: this is a message from the make telling you that it does not know how to build it. A 'clean' might help, see No rule to make target | MCU on Eclipse
Erich
Dear Erich,
I have tried all of them and still issue persists. Basically this is what I am trying to do. I generate a demo app from Beekit for CW10.6 Then without opening it from CW I open with KDS and convert it to CW project. Then, follow instructions to make sure include path is correct and all other steps. [adding rt in library and so on ..] basically I am still getting same error.
Do I need any application file which is .elf?
I tried creating a new project in KDS and I found a .elf file under binary on the top of the project list but here, there is no binary folder and no .elf file.
Please advise.
Thanks,
Salah
I got the same problem.
In my case, I had cancelled, using shell command, one source file from the kinetis project, but kinetis has not updated the makefile structure and looked for the missing C source.
To solve the problem, I've created, using shell command, the deleted file again, then close and reopened KDS, and remove that source file from kinetis.
In this way, kinetis has updated the makefile and now the compilation was success.
Using linux it's easier to use the preferred editor (vi, in my case) and shell commands, with the result that sometime KDS loose the control of the project, but this is acceptable.
Regards. Paolo