I'm trying to install the kinetis-design-studio_1.0.1-1_i386.deb.bin I downloaded on Ubuntu 12.04. Trying to run it as bin didn't work at all. I renamed it kinetis-design-studio_1.0.1-1_i386.deb and tried the dpkg install and it complains "The package doesn't provide a valid Installed-Size control field. See Debian Policy 5.6.20." Anyone else having this problem?
已解决! 转到解答。
OK I got it to work by ignoring the error when I simply double clicked on the package. I did have to rename it to remove the .bin suffix and then simply ran
dpkg -i kinetis-design-studio_1.0.1-1_i386.deb
in a shell.
OK I got it to work by ignoring the error when I simply double clicked on the package. I did have to rename it to remove the .bin suffix and then simply ran
dpkg -i kinetis-design-studio_1.0.1-1_i386.deb
in a shell.
To create a desktop shortcut you can do the following:
gedit .local/share/applications/opt_kinetis.desktop
Paste the following in to the edit window and save it:
[Desktop Entry]
Type=Application
Name=Kinetis-Design-Studio
Comment=Kinetis Design Studio
Icon=/opt/eclipse/icon.xpm
Exec=/opt/Freescale/KDS_1.0.1/bin/kinetis-design-studio
Terminal=false
Categories=Development;IDE;Java;
StartupWMClass=Eclipse
Open it with nautilus:
nautilus ~/.local/share/applications
right click on it, select properties, select the permissions tab, click "Allow executing file as program"
alternatively just do "chmod +x ~/.local/share/applications/opt_kinetis.desktop"
right click again and select "Make Link"
Drag the link to the desktop.