KDS IDE 2.0.0 and KSDK 1.1.0 support for KL17Z256

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KDS IDE 2.0.0 and KSDK 1.1.0 support for KL17Z256

Jump to solution
982 Views
StanleyH
NXP Employee
NXP Employee

Hello,
  Our customer, Foxconn, created an IoT Freezer platform project on Dec. 2014. They selected MKL17Z256VLH4 and scheduled to get PCBA sample out on Feb. 2015. They are designing schematic and firmware now.
  We use KDS IDE 2.0.0 and KSDK 1.1.0. After used "Installed New Software" KL27Z-1.0.0-GA-SA-Alpha-RC2.zip to add KL17 MCU support patch, we created a new KDS poject and found there are olny for 32 and 64KB, no 256KB in the processor selection list.
  Is there a patch for 256KB now ? 

  Are the sample codes in the \demo folder of the KL27Z-1.0.0-GA-SA-Alpha-RC2.zip also okay for KL17 ? Or are there sample codes dedicated for KL17 ?

Thanks.

 

18337_18337.pngpastedImage_1.png

 

Best regards,

Stanley

Labels (1)
Tags (4)
0 Kudos
Reply
1 Solution
561 Views
Rick_Li
NXP Employee
NXP Employee

Hi StanleyH,

Please download standalone installer of KL43 and KL03 from the below link

Software Development Kit for Kinetis MCUs|Freescale

(Please select "All Downloads" in the left and then download the standalone instaler for KL03Z and KL43).

After installed, you will see there is a subfolder with name "tools" in the installed folder.

there is a zip file in "eclipse_update" in this folder.

then, launch your KDS, click "Help"->"Install new software", in the launch window, click "Add..." button and then click "Archive..." to browse the zip file mentioned in above.

then, you can install this folder.

you need repeat the above process for both KL43 and KL03.

Hope it helps!

View solution in original post

0 Kudos
Reply
2 Replies
562 Views
Rick_Li
NXP Employee
NXP Employee

Hi StanleyH,

Please download standalone installer of KL43 and KL03 from the below link

Software Development Kit for Kinetis MCUs|Freescale

(Please select "All Downloads" in the left and then download the standalone instaler for KL03Z and KL43).

After installed, you will see there is a subfolder with name "tools" in the installed folder.

there is a zip file in "eclipse_update" in this folder.

then, launch your KDS, click "Help"->"Install new software", in the launch window, click "Add..." button and then click "Archive..." to browse the zip file mentioned in above.

then, you can install this folder.

you need repeat the above process for both KL43 and KL03.

Hope it helps!

0 Kudos
Reply
561 Views
StanleyH
NXP Employee
NXP Employee

It works. Thanks a lot!!

0 Kudos
Reply