I imported a KDS 2.0 project into KDS3, and went through the upgrade assistant, but I get a message saying Processor Expert is not loaded. Do I need to make a new Processor Expert project and apply all my existing settings? That would be a little painful.
Getting closer, now I see all my tasks and the settings with them. When I built, I got the note about updating lots of code for MQX. Now it's complaining about mke06z4.h on this line, saying INT_ADC is undeclared:
#define INT_ADC0 | INT_ADC |
Code generation is enabled, but is there something it needs to do to update this header?
Never mind, I clicked on "project" and "generate Processor Expert code", which seemed to update the header. Seems that the enum for that interrupt changed names, so it took a minor change to the code to change INT_ADC to INT_ADC0. Also took some fiddling with the P&E driver, since KDS 3 apparently ran into trouble installing the P&E drivers. Thanks Erich!