FRDM-K82F

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FRDM-K82F

2,891 Views
kentachang_melt
Contributor II

Hello,

I am interesting to FRDM-K82F and buy it. but I try to use KDS 3.0.0 create a new project, and then I have problem.

please let me know How to create and program the FRDM-K82F and then debug my project ?

Best Regards,

Kenta 

Labels (1)
0 Kudos
Reply
10 Replies

2,308 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Kenta,

Please check the computer management , if it show the "mbed serial port" like this :

pastedImage_0.png

when you debug , please select the "GDB OpenOCD Debugging" :

pastedImage_1.png

if PE , select the "GDB PEMicro " , if Jlink , please select "GDB SEGGER J-Link".

You can also refer to this DOC to know more about the three debug methods :

Summary of FRDM-K22F debug interface

If still can not work , please take a screenshot about the PC management and show it to me .

Hope it helps


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,308 Views
kentachang_melt
Contributor II

Hi Yang,

Can I use the Kinetis Design Studio 3.0.0 to route my firmware ? And download firmware into FRDM-K82F by USB Multilink , and then debug it ?

Regards,

Kenta

0 Kudos
Reply

2,308 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi Kenta,

What about your firmware?

The firmware i mentioned is the bootloader for debug , and only need one usb cable .

Please take a picture about  how your board link to PC and the configuration of KDS debugger,

that i can clearly know your meaning.

And please also tell me which debug method do you want to use , or your aim , thank !

BR

Alice

0 Kudos
Reply

2,308 Views
kentachang_melt
Contributor II

Hello Alice,

Is there any update for me?

Regards,

Kenta

0 Kudos
Reply

2,308 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello  Kenta,

I have test it use the MULTILINK , it can work well .

- Please first change the bootloader  of the board , for  example , you can change it to jlink

use the "JLink_OpenSDA_V2_1.bin" .

- then connect the board ,debugger to PC :

pastedImage_0.jpg

then check the PC management , whether have the USB Multilink:

pastedImage_2.png

Then configure the debug configuration as this :

pastedImage_1.png

Then it can download well :

pastedImage_3.png

Hope it helps


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

2,308 Views
kentachang_melt
Contributor II

Hi Alice,

1) Can I create a project (Kinetis Design Studio 3.0.0) for FRDM-K82F ?

2) Can you send a example project of FRDM-K82F for me ? I want to learn it use MULTILINK.

I hope to understand : my FRDM-K82F can work well, and then I can create a new firmware project.

Please …

Regards,

Kenta

0 Kudos
Reply

2,308 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Oh Kenta ,  you have not project ? So how do you test it before ?

Please download the KSDK2.0 project for FRDM-K82, then you can use it on KDS3.0.

About the detail method to download please refer to :

https://community.freescale.com/docs/DOC-329662

Hope it helps

Alice

0 Kudos
Reply

2,308 Views
kentachang_melt
Contributor II

Hi Alice,

the KSDK2.0 project is download, But I can’t use it on KDS 3.0.

Kenta

0 Kudos
Reply

2,308 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Kenta,

Pleas select the  SDK folder ,  it is the path of SDK_2.0_FRDM-K82F on you PC.

pastedImage_0.png

please refer to the video i mentioned last time : https://community.freescale.com/docs/DOC-329662

in this thread , there is the detail massage about how to use it .

Hope it helps you

Alice

0 Kudos
Reply

2,308 Views
kentachang_melt
Contributor II

Hi Alice,

I hope to program the FRDM-K82F by USB Multilink (SWD port).

The picture is attached.

May I have something wrong.

Regards,

Kenta

0 Kudos
Reply