I am using the KDS 3.2.0 and currently have nice working project built using the processor expert based on the MKE202Z64VLC4. I want to change it from this 64K Flash memory part to the MKE202Z16VLC4 version (which is the 16K variant). However, I have not found a way to change it. The two devices are the same with the exception of the 16K versus 64K one. Is there a way to change it in the KDS? (It would be time consuming to start all over again).
Thanks,
Bill
解決済! 解決策の投稿を見る。
You can change the pinout in the CPU component like this: https://mcuoneclipse.com/2012/08/16/changing-the-cpu-with-processor-expert/ (description for ColdFire, but same applies to Kinetis/ARM).
Another one on this subject is here: https://mcuoneclipse.com/2016/06/25/switching-the-microcontroller-package-device-and-family/
I hope this helps,
Erich
You can change the pinout in the CPU component like this: https://mcuoneclipse.com/2012/08/16/changing-the-cpu-with-processor-expert/ (description for ColdFire, but same applies to Kinetis/ARM).
Another one on this subject is here: https://mcuoneclipse.com/2016/06/25/switching-the-microcontroller-package-device-and-family/
I hope this helps,
Erich