程序编译过程中,出现以下报警信息,不确定哪个过程出现问题,望解惑,谢谢!

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

程序编译过程中,出现以下报警信息,不确定哪个过程出现问题,望解惑,谢谢!

988 次查看
mjliu
Contributor I

QQ图片20170920104857.pngQQ图片20170920104906.pngQQ图片20170920104910.png

0 项奖励
回复
3 回复数

883 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello MJ liu,

Do you use the demo board TRK-KEA128?

If yes, please first update the fimware  of your board:

1)Press the Reset button (and keep it pressed) while power the board with the OpenSDA USB connector(J16):.
2)  The board will
show up as BOOTLOADER drive on your system:
3) Copy" MSD-DEBUG-TRK-KEA128_Pemicro_v118 "
(I attached it for you) to the BOOTLOADER driver:
4) The copy operation takes about 2-3 seconds, after finished , unpower
 the board.
5) Power the board again normally .

Then in the debug configure view, please choose like below:

pastedImage_1.png

Hope it helps


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

883 次查看
mjliu
Contributor I

Hello,

very glad to receive your reply!

But, are you saying that the attachment will be another hair, but I'm still not yet received, so I can't make the following operation..

so.can you help me? 

                                    Have a great day,

0 项奖励
回复

883 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi MJ,

Please see my attachment .


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复