Hello MJ liu,
Do you use the demo board TRK-KEA128?
If yes, please first update the fimware of your board:
1)Press the Reset button (and keep it pressed) while power the board with the OpenSDA USB connector(J16):.
2) The board will show up as BOOTLOADER drive on your system:
3) Copy" MSD-DEBUG-TRK-KEA128_Pemicro_v118 "(I attached it for you) to the BOOTLOADER driver:
4) The copy operation takes about 2-3 seconds, after finished , unpower the board.
5) Power the board again normally .
Then in the debug configure view, please choose like below:
Hope it helps
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,
very glad to receive your reply!
But, are you saying that the attachment will be another hair, but I'm still not yet received, so I can't make the following operation..
so.can you help me?
Have a great day,
Hi MJ,
Please see my attachment .
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------