I am starting to work with MCUXpresso JLink Debugging of the FMU firmware. I am having trouble getting the debugger hit a breakpoint at the main function in the FMU firmware after flash loading, or to show me where in the source code the microcontroller is when the microcontroller is halted. It is not working as debug probe which is really disappointing since I have code I would like to debug! I am using the VirtualBox machine with the provided edu JLink. Can you help me?
解決済! 解決策の投稿を見る。
We are working on a tutorial video and will make it available in the community.