My JLINK debugger isn't working right. I can't set a breakpoint.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

My JLINK debugger isn't working right. I can't set a breakpoint.

Jump to solution
1,446 Views
nxf58541
NXP Employee
NXP Employee

I am starting to work with MCUXpresso JLink Debugging of the FMU firmware. I am having trouble getting the debugger hit a breakpoint at the main function in the FMU firmware after flash loading, or to show me where in the source code the microcontroller is when the microcontroller is halted. It is not working as debug probe which is really disappointing since I have code I would like to debug! I am using the VirtualBox machine with the provided edu JLink. Can you help me?

0 Kudos
1 Solution
1,407 Views
nxf58541
NXP Employee
NXP Employee

We are working on a tutorial video and will make it available in the community.

View solution in original post

0 Kudos
1 Reply
1,408 Views
nxf58541
NXP Employee
NXP Employee

We are working on a tutorial video and will make it available in the community.

0 Kudos