I'm having a problem with my ESC or Motor. What should I do?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

I'm having a problem with my ESC or Motor. What should I do?

跳至解决方案
1,989 次查看
nxf58541
NXP Employee
NXP Employee

Need some troubleshooting help. I have a motor that spins fine without the propeller on it, but will not spin once I put the weight of the propeller on it. I installed a new motor at that location and the new motor has the same behavior. I've checked all the connections on the ESC and power distribution panel and can't find anything wrong.

0 项奖励
回复
1 解答
1,918 次查看
nxf58541
NXP Employee
NXP Employee

If you think it's the ESC, which it sounds like it may be, NXP will do an RMA for just that part. 

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,919 次查看
nxf58541
NXP Employee
NXP Employee

If you think it's the ESC, which it sounds like it may be, NXP will do an RMA for just that part. 

0 项奖励
回复