I'm working on a GUI project and was planning to use LVGL which i know can run without an OS. My project is not complex so Id rather start without an OS. I wanted to use GUI Guider to speed up development but the options (I'm using mimxrt1050-evkb) show the OS as FreeRTOS. My questions are:
If I wish to incorporate the generated code into a project will it have FreeRTOS dependencies?
If so, can I set up GUI Guider so not use an OS?
Not the end of the world but would like to avoid OS is possible lol
Thanks!
已解决! 转到解答。
Hi,
Currently GUI Guider supports build-in FreeRTOS-based build and deploy for target board, the source code exported BY GUI Guider doesn't depend on FreeRTOS, it can support bare-metal usage.
Best Regards,
Zhenhua
Hi,
Currently GUI Guider supports build-in FreeRTOS-based build and deploy for target board, the source code exported BY GUI Guider doesn't depend on FreeRTOS, it can support bare-metal usage.
Best Regards,
Zhenhua
Hey Zhenhua,
Thanks for such a quick response. I've tested and looked through the generated code and understand how it works now. Its good to know that FreeRTOS is nota requirement of the generated code so i can continue with my work.
Kind regards and my thanks,
Lexi
Hi!
Have a look at the following stuff
https://github.com/gertvb/LPC55S69_GuiGuider
Basically gui guider on a bare metal lpc55s69