Upgrade issue - IFATAL ERROR - Removing earlier version while upgrading failed.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Upgrade issue - IFATAL ERROR - Removing earlier version while upgrading failed.

跳至解决方案
1,712 次查看
matejpacha_Ineltech
Contributor II

Hi,

I just tried an upgrade from previous 3.1 version to the latest, but I'm not successful.

The installation itself is started, then it tries to remove previous version, but that is the point when it fails.

The original folder is empty (seems to be removed), I also cannot see it in the system list of installed apps, but the new installer sees it somehow (probably in registers).

Is there any way to make a clean installation, overriding the registry check? Or which registers should I "remove" before the installation starts?

Thank you,

Best regards,

Matej

0 项奖励
回复
1 解答
1,697 次查看
iulian_stan
NXP Employee
NXP Employee

Hi @matejpacha_Ineltech,

Could you check this thread.

Hope it helps,
Iulian

在原帖中查看解决方案

2 回复数
1,689 次查看
matejpacha_Ineltech
Contributor II

Sorry for duplicated thread, I did search for it and did found nothing like that.

Thanks a lot!

Matej

0 项奖励
回复
1,698 次查看
iulian_stan
NXP Employee
NXP Employee

Hi @matejpacha_Ineltech,

Could you check this thread.

Hope it helps,
Iulian