MCAT motor parameter identification (see AN4986) missing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCAT motor parameter identification (see AN4986) missing

345 Views
HolgerMC
Contributor I

In AppNote AN4986 there is the detailed description of the motor parameter identification and the picture shows a special tab "Motor Identif".
MotorIdentif_AN4986.jpg
Even custom power boards are supported!

I want to use the S32K144 Evalboard with the DevKit MOTORGD and want to identify parameters of some unknown, small motors.
Where can this MCAT-functionality be found and which firmware is necessary to support this? Is it still available?

0 Kudos
Reply
0 Replies