Dear Quangui,
the free CodeWarrior license that you probably use only lets you to build applications up to 64k of code. You need to make the application smaller, or you need to get the full CodeWarrior license.
The FreeMASTER demo is quite large by default because it contains the whole project file and couple of HTML files and images compiled in the application for demonstration purposes. With this feature, you are able to load and open the project directly from the board Flash memory.
You may make the application smaller by turning off some features in the application's freemaster_cfg.h file:
Best regards,
Michal
Dear user,
An official S12Z driver and an example application for S12ZVMx12EVB board is available in "FreeMASTER Communication Driver" v2 package in the "downloads" section at www.nxp.com/freemaster.
A newer driver and example application which also supports protocol-v4 and all new features of FreeMASTER 3.0 is available unofficially. You can find it as fmstr-s12z-2019-12.zip attachment at this article.
Both driver versions contain UART and CAN examples and should work with FreeMASTER 3.0 out of the box. Be aware that a proper CAN bus termination is needed when running the demo at the default 500 kbps.
Best regards,
Michal
Hi Michal,
Thanks for your reply.
I have downloaded FreeMASTER3.0,but I can't find the example code.So I'm using fmstr-s12z-2019-12.zip attachment.
One error occured when I using the example code,and it can not be cleaned.please give me some advice.
Best regards,
quangui
Dear Quangui,
you are right, there was an absolute path to /project_settings/mc9s12zvml128.c in the .project file. You can edit the .project file, locate the path and change its entry to
<locationURI>PARENT-1-PROJECT_LOC/project_settings/mc9s12zvml128.c</locationURI>
or you can download a fixed zip file attached to the the original article. I have updated it there just a moment ago.
Regards,
Michal
Dear Quangui,
the free CodeWarrior license that you probably use only lets you to build applications up to 64k of code. You need to make the application smaller, or you need to get the full CodeWarrior license.
The FreeMASTER demo is quite large by default because it contains the whole project file and couple of HTML files and images compiled in the application for demonstration purposes. With this feature, you are able to load and open the project directly from the board Flash memory.
You may make the application smaller by turning off some features in the application's freemaster_cfg.h file:
Best regards,
Michal
Dear Michal,
Thanks for your reply.
I solved the problem according to your suggestion. Now the program can be downloaded to my board, but freemaster can not communicate with my ZLG usbcan_2e_u.Please see the pictures below.
In fact, my usbcan_2e_u can work with the cantest software, please see the picture below.
How can I solve this problem?
Best regards,
Quangui
I solved this problem by changing the ZLG software installation directory.We have to install ZLG in
C:\Program Files\CANTest .Although the identified hardware version number is wrong, it does not affect my use
Best regards,
Quangui
Dear Quanqui,
thank you for your latest update. The hardware device name is retrieved directly from the ZLG driver. Also in my case, it shows USBCAN-E for my USBCAN-2E-U device. I think this is a normal behavior.
Just FYI: You may still install the ZLG to a custom folder, you just need to set a path to this folder in FreeMASTER CAN plug-in configuration dialog.
Thanks,
Michal