Hi,
Today my Freemaster 3.2 doesn't want to work.. It crashes silently every time I launch it (also tried to launch from command line, in case there would be some error message there but nothing).
I have tried to uninstall and reinstall latest version from the website, problem persists.
I have used it a million times until two days ago. What could be wrong in my laptop that I should check?
Regards
Luca
已解决! 转到解答。
Hello Luca,
the issue should now be fixed. Please update to 3.2.2.2 available at www.nxp.com/freemaster
Please close this thread if you test the hotfix successfully.
Thanks,
Michal
Hello Luca,
yes as discussed in other two posts in this forum, the FreeMASTER Edge browser component crashes after a recent Windows/Edge update deployed by Microsoft. This issue affects all FreeMASTER 3.2.x versions with Edge support.
As Edge is the default component used to render the Welcome page, the FreeMASTER crashes as soon as you run it. When you run FreeMASTER by opening a project which uses IE or CEF engine to render HTML, then the FreeMASTER works normally (until you do File/New).
Another workaround is to rename the "c:\NXP\FreeMASTER 3.2\FreeMASTER\html" to html.bak to prevent the Welcome page to load. But still using Edge engine to render project-specific content may have issues.
We have identified the root cause of the issue and we are now working on hotfix release. This should be out during the next week - early Sep/2023.
Thanks for staying with us,
Michal
Hello,
We are experiencing the same issue
Freemaster last downloadable version on Win10 with last updates
HTML directory rename workaround does not work
Trying to open freemaster through a projet does not work either.
Are there other any fixes to test?
Dear Denis,
this seems to be a different issue than the Edge browser issue we were fixing in 3.2.2.2. Maybe partly related as the Edge internally uses Chromium engine, but we need to investigate.
Please open a new thread on this community and describe again. Also state if the issue can be replicated on multiple computers and/or if any computer exists which is not affected.
Thank you!
Michal