i.MX6(RSB4411-SBC)_ Boot_Prints_Issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

i.MX6(RSB4411-SBC)_ Boot_Prints_Issue

660 次查看
Devendra1
Contributor I

Hi All,

I am getting garbage prints in debug console(Board is booting properly) while booting with default images which comes with the board. With help of HDMI interface i can see kernel and u-boot version after board is booting.
       Kernel- version:4.1.15 
        U-boot version: 2016.03
Tried with different baud rates still issue is there.

Find below boot prints in minicom console for reference.

Welcome to minicom 2.8

OPTIONS: I18n
Port /dev/ttyACM0, 09:56:51

��w[}e�����q-{��YY^����ueݽ�-����sYgAYwoy����倭�WW�mw���53���������嵵���#1���;=7�y[y��-#1�753='�5#-#%5#����[������5='��a����5='��u���5='���WW�mw���53����������Y_^뺺ڿ������������s�������{��}��� 7�!�!�=!;!!�������￟��元�i�k�^�J #
�/5'��元��K.8���������}�gmS�����13;9�#�9!%%=#7��i�kl+�������5�3=-'57��YY^�5=7��75������;'!9)�����9!#����������;!!-#1�3%�-c}cw��k%-#1�!�U�{!!��ޯU�{!!�����������}�gmS�{�1;�3�59���e=��������������� o
�%�-!�'%�=���c!�!�75-95�755957���'��==A-#--='- �!#7�!�!'=15�5'59���'��%%9�75���-#-�3=-'57��_+�������������'!���!���q;����-%'�Y}W}�%!75���'=1��#9�=1 '

Devendra1_0-1686803760712.png


Thanks in Advance!

 

0 项奖励
回复
0 回复数