evkmimxrt1160 fails to find target.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

evkmimxrt1160 fails to find target.

跳至解决方案
1,613 次查看
JSuciu
Contributor II

After trying to manipulate TCM bank numbers, I am now unable to program the target. I moved to the hello world sdk project and unable to find the target. Did I brick the processor? See attached images.

0 项奖励
回复
1 解答
1,586 次查看
JSuciu
Contributor II

@kerryzhou,

 

Looking back through my debugging, I did set DTCM to 0 like you explained below (debugger flashloader no space to download the code). Can I push code to somewhere else to allow me to revive the processor?

Working through the document above (https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/RT-board-recovery-for-debugger-connect-issues/ta...), it didn't allow me to connect to the processor. I worked through both the IDE using the Erase Flash using LinkServer and using the MCUXpresso Secure Provisioning tool. I attached the error messages below but in short I am unable to find the target. This seems like an internal fuse blown, but want to confirm that. Is their an easy way to confirm that using the IDE or are the error messages attached allow me to find another way to wipe flash? Is their a special configuration off DIP switch SW1 to allow an ability to wipe flash memory.

Image_3 and Image_4 - Attempting to use the LinkServer Erase Flash tool

Image_5 - Attempting to connect to the target using the Secure Provisioning tool

Any help would be appreciated.

 

Thanks,

Jake

在原帖中查看解决方案

0 项奖励
回复
4 回复数
933 次查看
JSuciu
Contributor II

Hi Kerry, @kerryzhou 

I have ran back into this issue again. This is the errors that I get when attempting to debug through the linkserver.

JSuciu_0-1714423981814.png

 

I am able to find the probe through the Redlink Server. During debugging/flashing of the compiled code I get this notification from the console. 

JSuciu_1-1714424015969.png

I attempted all of the tasks above and it doesn't work to allow me to reflash code. 

 

If their is any other ways to get access to the target, it would be greatly appreciated.

 

Thanks,

Jake

0 项奖励
回复
931 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @JSuciu ,

Enter the serial download mode, then  power off and power on the board again.
If you still have issues about it, you can use the MCUBootutility, use this tool connection and do the mass erase in the serial download mode, I believe it's OK, otherwise, your board my have issues.
The MCUBootutility download link is:
https://github.com/JayHeng/NXP-MCUBootUtility/releases/tag/v6.2.0
the related user manual is:
https://github.com/JayHeng/NXP-MCUBootUtility

kerryzhou_1-1714471774138.png

 

Wish it helps you!

Best Regards,

Kerry

 

0 项奖励
回复
1,587 次查看
JSuciu
Contributor II

@kerryzhou,

 

Looking back through my debugging, I did set DTCM to 0 like you explained below (debugger flashloader no space to download the code). Can I push code to somewhere else to allow me to revive the processor?

Working through the document above (https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/RT-board-recovery-for-debugger-connect-issues/ta...), it didn't allow me to connect to the processor. I worked through both the IDE using the Erase Flash using LinkServer and using the MCUXpresso Secure Provisioning tool. I attached the error messages below but in short I am unable to find the target. This seems like an internal fuse blown, but want to confirm that. Is their an easy way to confirm that using the IDE or are the error messages attached allow me to find another way to wipe flash? Is their a special configuration off DIP switch SW1 to allow an ability to wipe flash memory.

Image_3 and Image_4 - Attempting to use the LinkServer Erase Flash tool

Image_5 - Attempting to connect to the target using the Secure Provisioning tool

Any help would be appreciated.

 

Thanks,

Jake

0 项奖励
回复
1,592 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @JSuciu ,

 Don't worry, you won't brick the processor, unless you burn the fuse.

Now, your issues is download the invalid image to the flash cause the boot issues, you can follow my document to recover it:

https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/RT-board-recovery-for-debugger-connect-issues/ta...

When you do the TCM configuration, please to avoid the ROM used TCM, 

kerryzhou_0-1710828729145.png

You also need to care about the flashloader used TCM, eg, the flashloader in the DTCM, but you set the DTCM=0, then you also will meet the issues, as the debugger flashloader no space to download the code.

 

Wish it helps you!

If you still have question about it, please kindly let me know.

If your question is solved, please help to mark the correct answer, just to close this case.

Best Regards,

Kerry

0 项奖励
回复