I acquired software FlexCan for DSC ( DLP-568-CX-FLXCN) and lack examples.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I acquired software FlexCan for DSC ( DLP-568-CX-FLXCN) and lack examples.

1,166 Views
robinsoncoutinh
Contributor I

Hi,

I acquired software FlexCan for DSC ( DLP-568-CX-FLXCN) for MC56F84xx. It has all the functions but has no way to use. For example, have the Send and Read function, but how should I use?

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

1,013 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

As far as I know, the example code DLP-568-CX-FLXCN developed based on PE needs dedicated CAN module license, which is not free. After you get license, you can get the code.

another engineers gave you the example code without license, I think it is okay.

0 Kudos
Reply