Can  "USB TAP for ONCE DSC" be used to device MC56F827xx ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can  "USB TAP for ONCE DSC" be used to device MC56F827xx ?

1,622件の閲覧回数
zhoujx
Contributor I


Hi, "USB TAP for ONCE DSC" cab be used to simulator 56F824x-5x via interface JTAC, but i don't know it can be used to simulator the new device MC56F827xx too.

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,271件の閲覧回数
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

The USBTAP device can be used to simulate the old DSC, for example MC56F83xx, MC56F80xx, MC56F82xx(MC56F8246, MC56F8257...), MC56F82xxx(MC56F82748....), MC56F84xxx(MC56F84789...).

But the USBTAP device can not be used to simulate the latest DSC family, for example, MC56F83xxx(MC56F83789), MC56F81xxx(MC56F81748) do not support USBTAP device, you have to use third party Multilink Universal device from PE Micro company:

www.pemicro.com

You can use CodeWarrior for MCU ver11.x to download and debug for the all above DSC family.

https://www.nxp.com/design/software/development-software/codewarrior-development-tools/codewarrior-l...

 

 

Hope it can help you

BR

XiangJun Rong

 

0 件の賞賛
返信

1,276件の閲覧回数
AnanthuRG
Contributor I

Will it also supports MC56F81xxx series?

0 件の賞賛
返信

1,486件の閲覧回数
larryyang
NXP Employee
NXP Employee

Yes, USB TAP JTAG OnCE also supports MC56F827xx.

0 件の賞賛
返信