Can  "USB TAP for ONCE DSC" be used to device MC56F827xx ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can  "USB TAP for ONCE DSC" be used to device MC56F827xx ?

1,442 Views
zhoujx
Contributor I


Hi, "USB TAP for ONCE DSC" cab be used to simulator 56F824x-5x via interface JTAC, but i don't know it can be used to simulator the new device MC56F827xx too.

Labels (1)
0 Kudos
Reply
3 Replies

1,091 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi,

The USBTAP device can be used to simulate the old DSC, for example MC56F83xx, MC56F80xx, MC56F82xx(MC56F8246, MC56F8257...), MC56F82xxx(MC56F82748....), MC56F84xxx(MC56F84789...).

But the USBTAP device can not be used to simulate the latest DSC family, for example, MC56F83xxx(MC56F83789), MC56F81xxx(MC56F81748) do not support USBTAP device, you have to use third party Multilink Universal device from PE Micro company:

www.pemicro.com

You can use CodeWarrior for MCU ver11.x to download and debug for the all above DSC family.

https://www.nxp.com/design/software/development-software/codewarrior-development-tools/codewarrior-l...

 

 

Hope it can help you

BR

XiangJun Rong

 

0 Kudos
Reply

1,096 Views
AnanthuRG
Contributor I

Will it also supports MC56F81xxx series?

0 Kudos
Reply

1,306 Views
larryyang
NXP Employee
NXP Employee

Yes, USB TAP JTAG OnCE also supports MC56F827xx.

0 Kudos
Reply