I use the CodeWarrior 7.2 and use the tblcf_gdi.dll.When I debugged,an error occured.
The Attachment shows the error.Who can help me?Thanks very much.
解決済! 解決策の投稿を見る。
Hi,
Read and respect then "CodeWarrior setup" of this document
See attached file
Sergio
Do you have the proper driver for the JB16 based TBLCF for CFV2 in CW7.2?
Hi
As explained in CodeWarrior setup in "Edit" "Preferences" "Remote Connection" , your named
TBLCF Connection have to point to tblcf_gdi.dll and not to USBDM_GDI_CFVx.dll by cliking on "Change" and browsing
to your tblcf_gdi.dll in the correct repertory.
Your attached file show CW7.2 looking for USBDM_GDI_CFVx.dll instead of tblcf_gdi.dll.
It works perfectly for me with JB16 TBLCF
Voici tout
With CW7.2, there is no TBLCF repertory under \Program Files\Freescale\CodeWarrior for ColdFire V7.2\bin\Plugins\Support\ColdFire
Freescale supplies only Abatron, OSBDM and PEMicro repertories.
Where have you found all your TBLCF files ?
Then what's the version of CW that you are using for coldfire V2?
Hi
I'm using TBLCF for Coldfire V2 MCF52236 and MCF5271 with CW7.1 or CW7.2 with success
I am wrong.Now I know those files are not tblcf files.They are for TBDML,not for JB16 based TBLCF.
Bestregards
zipper
I made a folder named tblcf.Maybe tblcf does not work in CW7.2.I will try it in CW7.1.Thank you very much.
Bestregards
zipper
Hi,I did as what you said,but it still won't work.I found a lot of dlls and none could work properly.I think my driver for the TBLCF may not be corrretly installed.Do you have the driver for TBLCF?I can't find other driver on the Internet.
Bestregards
zipper
Do you have the proper driver for the JB16 based TBLCF for CFV2 in CW7.2?
Hi,my device is TBLCF that is based on JB16 for CFV2,I got a driver and installed it.But the CW7.2 can't dectect it.