No probe connection for Codewarrior Tap

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

No probe connection for Codewarrior Tap

980 Views
cengizhanyapici
Contributor I

In my bareboard application I want to use Codewarrior development studio although when I create a new project and debug it I take an error which is "CCSProtocolPlugin:Could not connect to the probe(or other debug link)

[CCS last error:CC not present ]"

Then,I run the necessary COM port from TerraTerm application and I see "No probe connection" message on the screen.Is the problem related to this "No probe connection" message which is given as attached? or Is there some problem about CodeWarrior's connections? Thanks for your answers.

 

Best Ragards

Labels (1)
0 Kudos
Reply
1 Reply

676 Views
addiyi
NXP Employee
NXP Employee

What connection you are setting in CW for cwtap?

Adrian

0 Kudos
Reply