Hi June,
Thanks for your reply, I have a follow-up question, when I create an attach configuration it seems that the 10.5.1 doesn't support the use of USB TAP for t1040qds. I can only select CodeWarrior TAP (over USB), CodeWarrior TAP (over eth), Gigabit TAP or Gigabit TAP +Trace. While for t2080, I can select the Connection Type as USB TAP. I only have a USB TAP debugger. Is there a version that supports the use of USB TAP debugger on t1040?
BRs
Minghu.