Does CW PA v10.3 support t1040 boards?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does CW PA v10.3 support t1040 boards?

Jump to solution
1,561 Views
minghu_du
Contributor III

As title, does CW PA v10.3 support t1040 boards?

I can only create  Codewarrior Bareboard project for QorIQ P1/P2/P3/P4/P5 T4 boards, what about T1 series?

 

Image20221008153803.png

I want to debug my T1040qds, but I'm not able to create a project for T1 series.

 

0 Kudos
1 Solution
1,539 Views
June_Lu
NXP TechSupport
NXP TechSupport

Please use NXP  CodeWarrior 10.5.1 to create T1 series project.

View solution in original post

0 Kudos
4 Replies
1,523 Views
June_Lu
NXP TechSupport
NXP TechSupport

The case has been closed, please raise a new case to get the answer. 

0 Kudos
1,535 Views
minghu_du
Contributor III

Thanks.

0 Kudos
1,540 Views
June_Lu
NXP TechSupport
NXP TechSupport

Please use NXP  CodeWarrior 10.5.1 to create T1 series project.

0 Kudos
1,530 Views
minghu_du
Contributor III

Hi June,

Thanks for your reply, I have a follow-up question, when I create an attach configuration it seems that the 10.5.1 doesn't support the use of USB TAP for t1040qds. I can only select CodeWarrior TAP (over USB), CodeWarrior TAP (over eth), Gigabit TAP or Gigabit TAP +Trace. While for t2080, I can select the Connection Type as USB TAP. I only have a USB TAP debugger. Is there a version that supports the use of USB TAP debugger on t1040?

BRs

Minghu.

 

 

0 Kudos