CW6.3 Special Edition for Coldfire

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CW6.3 Special Edition for Coldfire

6,138 Views
hdj100r
Contributor I
I have the CW6.3 which came with my M52235EVB. I thought this had a non time limited special license for 128K. Now when I start up CW it says I have 25 days until the current license expires.
 
Do I have to register it?  No registration number came with EVB.
 
David
Labels (1)
0 Kudos
Reply
18 Replies

2,047 Views
CrasyCat
Specialist III

Hello

CodeWarrior for Coldfire V6.3 has not been released yet (as far as I know).

We do not provide registration code for bet software. You will have to wait until V6.3 is official to get your permanent license file.

CrasyCat

0 Kudos
Reply

2,047 Views
hdj100r
Contributor I
Hello,
 
With my EVB I got last month, I received CodeWarrior V6.3, Special Edition, Preview Release, Part No 770-75504 Rev A.
 
My understanding was that this was a 128K code limited version, with no expiry date. If that is not the case, how do I get the "fully licensed, complimentary Special Edition of the CodeWarrior Development Studio for ColdFire Architectures for development of applications up to 128Kbytes code size" as promoted with the M52235EVB on the freescale web site?
 
Will there be non beta software released before the version shipped with the EVB expires?
 
David
 
 
 
0 Kudos
Reply

2,047 Views
DistiCasMgr
NXP Employee
NXP Employee

Hi,

I would suggest that you email your local FAE near to license expiry (around 5 days to go).

They can check whether V6.3 is about to release and if not arrange to issue a new 45 day license key.

Which country are you based in?

Do you already have a name of a local Freescale FAE? If not I can provide.

Thanks

0 Kudos
Reply

2,047 Views
hdj100r
Contributor I
Hi,
 
I am in Sydney, Australia. I will talk to local Freescale FAE.
 
Thanks
David
0 Kudos
Reply

2,047 Views
CrasyCat
Specialist III

Hello

I get some news from product manager. Final release of 6.3 (targeted for 7/21) will come with a permanent special edition key.

The special edition software will also be uploaded to our CodeWarrior for Coldfire download page.

CrasyCat

0 Kudos
Reply

2,047 Views
hdj100r
Contributor I


I get some news from product manager. Final release of 6.3 (targeted for 7/21) will come with a permanent special edition key.


Any news as to the final release of 6.3
 
Thanks
David
0 Kudos
Reply

2,047 Views
CrasyCat
Specialist III
Hello
 
CodeWarrior Development Studio for ColdFire Architectures v6.3 Update   is available for download from following URL:
 
CrasyCat
0 Kudos
Reply

2,047 Views
hdj100r
Contributor I

Thanks CrasyCat,

I did find that link, and have filled the request details in, but have heard nothing. How long does it take to process a request?

Thanks

David

 

 

0 Kudos
Reply

2,047 Views
CrasyCat
Specialist III

Hello

Did you press the download button next to "CodeWarrior for ColdFire Architectures v6.3  Release Date: 7/24/2006 " on the bottom of the page?

Is that working?

CrasyCat

 

0 Kudos
Reply

2,047 Views
hdj100r
Contributor I

Hi CrasyCat,

I don't have a download button. The message I get is :

CodeWarrior for ColdFire Architectures v6.3

Your request to download this item has been received and forwarded for review. A Freescale representative will contact you.Thank you for your interest in Freescale.


Click to return to the
COLDFIRE-UPDATES Product Summary Page

 

David

 

 

 

 

0 Kudos
Reply

2,047 Views
hdj100r
Contributor I
Hi
 
I finally, after two days!!,  got the information from the Software Download Admin to download.
 
Thanks
David
0 Kudos
Reply

2,047 Views
CrasyCat
Specialist III

Hello

Get a confirmation that this is a known issue and we are working on fixing that.

We are sorry about this delay.

CrasyCat

0 Kudos
Reply

2,047 Views
aprendiz
Contributor I
Hi, I've also got the EVB without the special Edition, but a time expire Professional Edition, now I'm looking for the Special Edition, in your last posts you wrote that this edition would be available at Freescale page, well, I got to this page:
 
 
and there is no link to download the special Edition, is this a an error? And where can I download the CodeWarrior Special v6.3 Special Edition for ColdFire?
 
thanks in advance for your effort and help.
0 Kudos
Reply

2,047 Views
CrasyCat
Specialist III

Hello

If you download and install an evaluation version of CodeWarrior for Coldfire V6.3, a special edition license is automatically installed in the root installation directory.

The special edition license is not available on the web. You are right.

I will contact marketing and check with them why it is not there.

CrasyCat

0 Kudos
Reply

2,047 Views
CrasyCat
Specialist III
Just an add on here.
The special edition will be installed automatically if you install Coldfire V6.3 evaluation software.
 
As the license if available in the installation, there is no need to place the license file on the web. Just install V6.3 and you should be able to use the special edition software.
 
CrasyCat.
0 Kudos
Reply

2,047 Views
aprendiz
Contributor I
Thank you CrasyCat, I've just downloaded and installed the Coldfire V6.3 evaluation software, it's working already. Thank you again. But it' would be great that you spread this issue.
0 Kudos
Reply

2,047 Views
aprendiz
Contributor I
Hi, I've also got the EVB without the special Edition, but a time expire Professional Edition, now I'm looking for the Special Edition, in your last posts you wrote that this edition would be available at Freescale page, well, I got to this page:
 
 
and there is no link to download the special Edition, is this a an error? And where can I download the CodeWarrior Special v6.3 Special Edition for ColdFire?
 
thanks in advance for your effort and help.
0 Kudos
Reply

2,047 Views
hdj100r
Contributor I

Thanks CrasyCat. That is good news.

David

 

0 Kudos
Reply