Hello
All upgrade and patches will be done for V4.5. We will not generate patches for V3.1 anymore.
You can continue to use your V3.1 software if you want, but new derivatives will be supported in the new release only.
CrasyCat
Hello
CodeWarrior for HC12 V3.1 cannot be downloaded from the web any more, but you can download CodeWarrior for HCS12X V4.5.
This software supports HC12, HCS12 and HCS12X cores.
To download the software go to following URL
http://www.freescale.com/webapp/sps/site/overview.jsp?nodeId=01272600612247
and click on the link CWX-H12SX-SE to download the software. It comes with a special edition license already installed. The special edition license will allow you to build up to 32K of C source code.
I hope this helps.
CrasyCat
marc.paquette wrote:Do you want access to the CodeWarrior HC12 3.1 tools? Do you want access to the updates & patches to these tools?
Yes! I'd like all downloads relating to previous versions of CodeWarrior to remain available on the website - even if Freescale is no longer supporting these products.
Steve Melnikoff.
CrasyCat wrote:CodeWarrior for HC12 V3.1 cannot be downloaded from the web any more, but you can download CodeWarrior for HCS12X V4.5.
Why not? What do Freescale have to lose by making it available?
As an example of why this might be useful, if you change your office PC, then you'll need to re-install CodeWarrior. That's fine if you can locate the CD it came on, but being able to download it would make life a lot easier.
Being able to upgrade to a new version is of no use to us (and, I suspect a lot of embedded systems designers), as when we release new versions of software for existing products, we would prefer to use the same compiler throughout the life of the product. Hence even if Freescale no longer support this version of the compiler, they should at least continue to make it (and any patches) available for download.
Steve Melnikoff.
Freescale is happy to continue to answer technical questions for CodeWarrior HC12 3.1 on this forum and through paid technical support.
To take advantage of new features and development tools for HC12, you'll have to pay for version 4.5.
If it's any consolation, Freescale includes 1 year of free support and a heavy discount for upgrades to CodeWarrior tools.
I just hope that I never need any new features then, because all those upgrades cost time and money, especially when you have an annoying "floating license". I would seriously concider getting a compiler from another company if I have to do it yet another time.
Perhaps I only have myself to blame for picking HCS12 when it was brand new. I won't make that mistake again... better to wait 3 years after a MCU release until all the bugs are sorted out and let somebody else pay for getting them solved.
Message Edited by Lundin on 2006-06-07 08:42 AM
Lundin wrote:Perhaps I only have myself to blame for picking HCS12 when it was brand new. I won't make that mistake again... better to wait 3 years after a MCU release until all the bugs are sorted out and let somebody else pay for getting them solved.