Hello,
I'm looking for a good alternative to debug the PowerPC microcontroller SPC5668E. One alternative would be to use CW 10.6 together with P&E Micro's debug probe (U-MULTILINK or U-MULTILINK-FX).
Does anyone have experience with this setup?
I would also like to know if an 14-Pin Berg to 38-Pin Mictor Adaptor (like http://www.pemicro.com/products/product_viewDetails.cfm?product_id=159 ) is included if I buy U-MULTILINK or U-MULTILINK-FX? I have a 38-pin mictor on the PCB.
What debug features are included in CW 10.6?
Can I set a breakpoint while the programming is running?
Can I get live update on variables?
Callstack?
Can I change variables etc.?
Write to HW registers?
Is trace included?
Can I program the device with CW 10.6?
Kind regards,
Jonas
已解决! 转到解答。
Hello Jonas
U-MULTILINK and U-MULTILINK-FX only has 14-pin JTAG interface, and the emulators supported by CodeWarrior does not has MICTOR Connector.
The 14-pin JTAG connector does not allow for trace information.
The MICTOR connector allows for full real-time trace to be supported, either program trace, ownership trace, or data trace.
The features that 14-pin JTAG Connecter supports:
- Full run control capabilities:
= setting breakpoints
= modifying memory
= step program execution
- Nexus Read Write Access - capability to read and modify memory while
target is running
- Access to last 8 branches taken (no instruction counts)
38-pin MICTOR (Full Nexus)
- All features available with 14-pin JTAG
- Program Trace - via branch trace with instruction counts
- Data Trace - Reads, Writes, or Reads and Writes
- Ownership Trace - if core OTR register is used to signal changes in
tasks/owners
- Watchpoint Messaging/Trace
I would suggest to contact P&E to get to know whether the above functionalities work well after the JTAG signal is converted by Mictor Adaptor.
Best Regards
Fiona Kuang
Technical Information & Commercial Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Jonas
U-MULTILINK and U-MULTILINK-FX only has 14-pin JTAG interface, and the emulators supported by CodeWarrior does not has MICTOR Connector.
The 14-pin JTAG connector does not allow for trace information.
The MICTOR connector allows for full real-time trace to be supported, either program trace, ownership trace, or data trace.
The features that 14-pin JTAG Connecter supports:
- Full run control capabilities:
= setting breakpoints
= modifying memory
= step program execution
- Nexus Read Write Access - capability to read and modify memory while
target is running
- Access to last 8 branches taken (no instruction counts)
38-pin MICTOR (Full Nexus)
- All features available with 14-pin JTAG
- Program Trace - via branch trace with instruction counts
- Data Trace - Reads, Writes, or Reads and Writes
- Ownership Trace - if core OTR register is used to signal changes in
tasks/owners
- Watchpoint Messaging/Trace
I would suggest to contact P&E to get to know whether the above functionalities work well after the JTAG signal is converted by Mictor Adaptor.
Best Regards
Fiona Kuang
Technical Information & Commercial Support
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Ok so NXP don't sell the adaptor that I refer to (http://www.pemicro.com/products/product_viewDetails.cfm?product_id=159)?
Is the microcontroller SPC5668E supported? I can't find it in the supported devices list. I can see that SPC5668G is supported.
Kind regards,
Jonas