Hi,
I am using a customized board with MK50DX256.
I want to use processor expert in CodeWarrior to use it as a device driver. I want to be able to use the serial function in hyperterminal through USB. Is there a bean in processor expert that would help me achieve that? Also any sample project would help?
Hello Kiran,
You can use the component of "USB_LDD".
After add this component , right click it , then select the "help on component " , then click "Typical Usage",
there is USB demo :
Hope it helps
Alice
Hello Kiran,
I think you have not enable the "clock pin":
Hope it helps
Alice
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Alice,
Hope you're doing well.
I wish you could provide me some help with this USB CDC DEVICE
I would appreciate it.
-Kiran Tujare
Hi Alice,
Can you answer this thread please?
https://community.nxp.com/message/826698
Hey Alice,
I wanted to direct you to this. Please reply.
Hi Alice,
I am doing a project for USB CDC using this link https://centaurian.co.uk/2015/12/23/ksdk-usb-cdc-printf/
I got it working for my board. I want to type on hyper terminal and I am not being able to do that. How do I make scanf work for that? Please reply in your spare time.
-Kiran
Hi ALice,
I installed USB Stack v4.1.1 NXP bare metal (no OS) USB Stack and imported USB_.PEupd components in the processor expert but I cannot view USB_AUDIO_CLASS.PEupd and USB_CDC_CLASS.PEupd because the processor expert filters these components. Is there a way to remove the filter. I have pointed out the place where it is filtered in the attached file
Hello Kiran,
1) You can disable the filtering :
2) If you use the PE component , there is demo code on the "help on component " i said above.
3) I see you use the chip of K53DN512 , you can also download the KSDK ,use the KDS IDE,
there are USB demo for TWR-K60D100, it is the same with mk53dn512 Chip .
You can refer to this thread to download and install KSDK v2.0 on KDSv3.2 :
Using Kinetis Design Studio v3.x with Kinetis SDK v2.0
when download KSDK, select the chip you used .
Hope it helps
Alice